STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1400 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 553 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32WL55CCUx debug mode issue in STM32CubeIDE v1.4.1

I am using STM32Cube IDE version 1.4.1 where I'm debugging 1st the CM4 Core which is getting debugged and then I tried to debug CM0+ core which is not going into debug mode and showing the error :Target unknown error 32Error in initializing ST-LINK d...

Somya by Associate II
  • 386 Views
  • 4 replies
  • 1 kudos

Resolved! Getting started with STM32CubeIDE

Hi I am just getting started with STM32CubeIDE for a project I am doing at my university!I have made an account and installed the software, and I got the board (NUCLEO-L552ZE-Q), I wanted to start a new project with the board to try and blink and LED...

STM32CubeIDE 2.1.0 released

We are pleased to announce that STM32CubeIDE 2.1.0 release is available. What is new in 2.1.0: Added support of STM32C5 seriesAdded support of new microcontrollers across the STM32WBA, STM32WL, STM32H5, STM32U3 and STM32F7 seriesAdded support of new ...

Aimen1 by ST Employee
  • 1517 Views
  • 0 replies
  • 1 kudos

STM32Cube IDE 1.16.1 unusable on Linux Mint 22

I recently updated to Linux Mint 22 (Cinnamon 6.8, kernel 6.8.0, Ubuntu 24.04) by means of the "generic Linux" version. (I had tried without success the Debian package and was advised to use the "generic" instead).The software works and compiles OK a...

feb by Associate
  • 4825 Views
  • 6 replies
  • 5 kudos

Multi Core Debug Problem, Single Core Debug OK

In an effort to track down an unrelated problem, I switched back to using my H7 DISCO board and the HSEM_CoreSync sample application. If I debug only the CM7 code, or only the CM4 code, I can step through any/all lines. However, if I try to multi-cor...

CCoder_0-1770136630625.png CCoder_1-1770136761175.png
C-Coder by Associate III
  • 322 Views
  • 3 replies
  • 0 kudos

SFR view crashes STM32CubeIDE

Whenever I try to use the SFR view window, it consistently crashes the IDE. Completely hangs up, not responding to anything (e.g. resizing the window) anymore.. left it sit for 15min (way too long) no responsiveness.I can easily reproduce this by lau...

Hans1990 by Associate
  • 4458 Views
  • 10 replies
  • 3 kudos