cancel
Showing results for 
Search instead for 
Did you mean: 

cube ide strange breakpoint behaviour

john_love_stm
Associate II

Using cube IDE to debug my application i've witnessed breakpoints behaving unpredictably: sometimes they appear on their own in breakpoint list view while not present in the file editing view; other times the breakpoints i've just placed and just used dissapear.
What can be a cause of such behaviour and how can i prevent it from happening?

6 REPLIES 6
Ghofrane GSOURI
ST Employee

Hello @john_love_stm 

First let me thank you for posting.

Could you please provide more details about the STM32CubeIDE version that you are using as well as your OS.

 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello, @Ghofrane GSOURI
First let me thank you for replying.
My OS is Windows 11 and my STM32CubeIDE version is 1.14.1.

Ozone
Principal III

Not a Cube IDE user, but ...

Are you sure the debug artifact and source code match ?
Have you tried a clean, and full rebuild ?

Hello @john_love_stm 

I recommend you to use the latest STM32CubeIDE version 1.18.1 rather than 1.14.1

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I don't think i understand your question. What do you mean by "debug artifact"?
Hard to tell if full rebuild would help since the issue happens randomly with and wihtout rebuilding

> I don't think i understand your question. What do you mean by "debug artifact"?

The ELF / HEX / BIN file created by the toolchain, which is executed on the target.
"Build artifact" is a common term for any files created during the build process.

> Hard to tell if full rebuild would help since the issue happens randomly with and wihtout rebuilding

This is somewhat difficult to judge from the outside.
Have you tried a different target board, or a different host PC ?

I would first try with copy of the project, either in another folder or on another PC. And perhaps a simple example project for your MCU.

Another option would be  Segger's Ozone (unrelated to my moniker here): https://www.segger.com/downloads/jlink/#Ozone
This is generic Cortex M debugger usable independant of any specific toolchain. Last time I checked, it was free for non-commercial projects. I'm not sure if it supports ST-Link directly, but you can reversibly flash a Segger firmware to onboard ST-Links to make it a J-Link.