STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1431 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Code Generation Bug STM32U5 with VDDA

Hello! I believe I found a code generation bug. I am currently using IDE version 1.16.1.By default, when enabling ADC with an STM32U5, HAL_MSPInit() has the line: HAL_PWREx_EnableVddA() which is necessary to have a positive reference for the ADCs (th...

rgangwan by Associate
  • 1903 Views
  • 2 replies
  • 3 kudos

Generating code for HTTPD in NUCLEO-H745ZI Board

Hi Team,"I am trying to configure an HTTP server on the Nucleo-H745ZIT6 board, which has two Cortex cores. I am using Cortex-M7 for this. After enabling HTTP in middleware inside LwIP, and generating the code, LwIP is placed inside the Cortex-M7 fold...

ggowd.1 by Associate III
  • 7643 Views
  • 5 replies
  • 0 kudos

Resolved! Unit testing and system initialisation code

I am currently working on testing of some code using a testing tool. As nearly all of the code interacts with the hardware, it is easiest for me to do this on the target. The tool automatically builds the test environment and allows files and/or func...

CTapp.1 by Senior III
  • 3537 Views
  • 8 replies
  • 2 kudos

Error when running Debugger in STM32CubeIDE

Hi,I want to load a program into my STM32U575 microcontroller using the STM32Cube IDE debugger.This is my Debug configuration:But when I run the Debug, I get the following error:        Why do I get this error and how can I fix it?Best regards,

1.png 2.png 3.png
mikel-m by Associate III
  • 2137 Views
  • 4 replies
  • 0 kudos