STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1409 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! TouchGFX - generated code - Screen1View

Hello,I am trying to learn a structure that is provided for MVP implementation. I dont understand where is Screen1View and every other class instance placed. I see that definitions are in .hpp files and implementations of .cpp file. Also, I am really...

richi by Associate III
  • 1887 Views
  • 3 replies
  • 0 kudos

Resolved! Stm32h746 dual core debugging

I am working with stm32h745ZIT3, in my application I need to receive some packets over ethernet in CM7 and these packets need to share to CM4, and processing is done in CM4. So, to test this data transfer I need to debug both cores simultaneously. Tr...

Jpj.1 by Associate II
  • 3440 Views
  • 7 replies
  • 0 kudos

Request for old stm32cubeIDE versions 1.14.0 and 1.15.0

Hi ST Community, I am using the board of STM32WBA55CGU6 board for OTA application and i want to use the application present in STM32Cube_FW_WBA_V1.3.0 and STM32Cube_FW_WBA_V1.2.0 packages. Since these packages are present in STM32Cube IDE version 1.1...

Shaku by Associate II
  • 1983 Views
  • 4 replies
  • 1 kudos

CubeMX generated code error when using BSP code

Hello all.I'm new here, this is my first post.I found a problem with STM32CubeIDE.I don't know where to post errors report, so please move this post if this is the wrong place.I'm a skilled embedded programmer, but I've worked till now on 8 bit micro...

Task runtime usage for ThreadX in STM32CubeIDE

Hi,In How to enable FreeRTOS™ Run Time and Stack Usage view, it shows we can see the task runtime usage in percentage for FreeRTOS. But for ThreadX, it has no such item.  As there is an 'execution_profile_kit' utility tool in ThreadX already, any pla...

Resolved! Yet another "Failed to execute MI command" problem...

Hi guysThis project here was built and debugged fine last week. Today, I get this message:'Launching has encounteres a problem. Error in final launch sequence: Failed to execute MI command: -environment-cd <Path/to/project> Error message from debu...

err msg.png
White_Fox by Associate III
  • 7821 Views
  • 5 replies
  • 3 kudos