User Activity

I update to V1.16 and found, that my project cannot compile anymore.Problem are compile errors, double definitions and so on. I did not change the code, just updated and regenerated everything include the code generation of CubeMX ( from within the i...
I have an older code where I use TIM1 in PWM2 mode to generate a frequency for a buzzer connected to the OC Channel4. Code is coming from F051 project.Now I started a new project and wanted to reuse the same principal, but i do not see the function t...
Hi, I want to transfer 64kByte of data from memory to my display controller using SPI and DMA.Everything is working smoothly so far, but I have some problems of understanding, when I try to use the max. number of bytes.So: 64kByte = 65536 Bytes.But t...
We have a battery driven system based on STM32G031K8 and a S2-LP for RF running from a CR2032.I use the shutdown mode to keep power as low as possible. System is done by a reed contact connected to a wake up pin.We want to find out, whether the batte...
Started today with my STEVAL-STWINKT1B, with default firmware and an outdated version of ST BLE Sensor app.I was happy, the app connected and I was able to do a first trial, gather some data and export the data as csv by email.After that, I did an up...
Kudos given to