STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 222 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Failed to read time and date in STMWLE5 software

I want to record the time of sensor activity in a program running in STM32WL MCU but only get the value of 0. The program is modified from the example LoRaWAN_End_Node. Below please find the RTC setting and the code to get the date and time. Can any ...

W.K. Tam by Associate III
  • 1684 Views
  • 2 replies
  • 0 kudos

wrong transmission through BLE data writing in STM32WB55

 I programmed a microcontroller to return received text data from BLE using UART.However, I can get only 4 alphabet clearly and the next alphabet becomes broken.For example, If I send the text "aaaaaa", then the microcontroller return "aaaa0(9)??" or...

KKIM.6 by Senior II
  • 880 Views
  • 0 replies
  • 0 kudos

STBox RTC time recording problem

Hello everyone,I encountered an issue while trying to record sensor data to an SD card using the sensorTile box. The sampling frequency is set to 50 Hz. However, upon checking the CSV file, I noticed that it only displays one decimal place after the ...

Screenshot 2023-08-07 125647.png
Junyan by Associate
  • 818 Views
  • 0 replies
  • 0 kudos

Problem FUS when I try to load BLE Stack on STM32WB15xx

Hi everyone.I have a problem when I try to load BLE Stack on STM32WB15. I can connected the MCU to STM32Programmer and there can recognize the cortex. At the moment to load the Stack, STM32Programmer send me the configuration about FUS and I cand rea...

0693W00000JPIHGQA5.png
JCALD.1 by Associate II
  • 3169 Views
  • 5 replies
  • 1 kudos

FUS file is missing for STM32WB1x

Hi,We use STM32WB15CC for our projects and some MCU's FUS version are 0.0.0.So we want to try re-program FUS file to MCU.While we checked STM32CubeWB, there are FUS files for STM32WB3x and STM32WB5x in "STM32WB_Copro_Wireless_Binaries" folder, but no...

batuars by Associate III
  • 8408 Views
  • 16 replies
  • 0 kudos

SPIRIT1 Relevant issues regarding

"Using SPIRIT1 to transmit packets. I need an empty command (like NOP). Will it be generated automatically, or do I need to add it manually? I didn't find any relevant explanation in Datasheet. Also, can FEC be manually disabled?" 

hsu77777 by Associate
  • 1095 Views
  • 0 replies
  • 0 kudos

Can't upgrade Firmware on NUCLEO-WB15CC

I am trying to upgrade my Nucleo board to Wireless firmware stack v1.17.0 from GitHub (Address: 0x08021000), but I always get the Warning:FUS_STATE_ERR_UNKNOWN after upgrading.And when I try to start FUS, I get:Error: FUS_STATE_ERR_UNKNOWN: Unknown e...

tester by Associate III
  • 1896 Views
  • 4 replies
  • 1 kudos

How to make larger STM32WB55 ZigBee Neighbours Table size

Hi.I am working on a ZigBee project for the STM32WB55. I use Zigbee wireless binary of STM32Cube_FW_WB_V1.16.0 as below.stm32wb5x_Mac_802_15_4_fw.bin, stm32wb5x_Phy_802_15_4_fw.bin, stm32wb5x_Zigbee_FFD_fw.bin. It works well for now with using zigbee...

JayRullia by Associate II
  • 1008 Views
  • 1 replies
  • 0 kudos