NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello members,Please let me ask about how to use external SIM on B-L462E-CELL1.I inserted the plastic SIM to external SIM slot on B-L462E-CELL1.Then, I set APN and confirmed it get ICCID from SIM.However, I dont make clear how to setup connect networ...
Hello,i am designing a custom board with the stm32WL55.i saw the MB1789 schematic and design, and i need to know more about this configuration and what are the advantage and inconvenient ?in this design they don't have a switch and the same line is u...
Hi, I'm using a STM32WLE5CCU micro with FW_WL V1.3.0 library. I want to implement a feature that receives a downlink command from the Network Server and reboot the entire system like pushing a reset button will do.Once the command is received, is the...
Dear all,I would like to communicate regarding character read and write from STBLEToolBox using P-NUCLEO WB55.May I ask would you be available to communicate regarding location where would I could find variable on the IDE and make usage on a function...
How can I get to scenes and groups data stored in device after receiving add command?
Hello ST!GOOD day,We are looking new MCU for VOIP [voice over Internet protocol] project that can handle Internet connectivity and Communications ADC, UART] [, LAN, WAN, FXS, FXO support]. can you suggest MCU's for best and available MCU.with Wi-Fi 5...
Hi,I configured USB FS on my STM32WB55 NUCLEO Board and it works as I expected (configured as CDC). I can send and receive data to/from Host (my PC) but now I have the need to suspend temporarly Data Flow and then reprise it.My goal is to collect som...
We are looking to use the STM32WB5MMG to measure a few seconds of data, then transmit that over bluetooth.We have managed to get the current consumption of the internal ADC during this measurement down to around 500 uA using low power sleep mode, how...
!!Naive question!!I have started LoRa development recently, I am using RAK3172 module which has STM32WLE5CCU6 embedded with it. Now during the development, I am seeing that the module is transmitting and joining the server but it is not getting any j...
I tried to design a board using the STM32WLE5CCU6, so I referred to the reference designs MB1720,1842,1848, etc.However, I confirmed that the VDDRF part, which is the part specified in the data sheet, is open with the SB connector.I searched for the ...