NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Error: ST-LINK error (DEV_TARGET_CMD_ERR) Error: Device not supportedflash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x0.stldr is loaded
I see a lot of reference to VirtualWire or RadioHead library for using RF433Mhz ISM band links. But I haven't find a library for KEIL ARM MDK using CubeMX or HAL drivers.
i need a development board of STM32WB. From where i can purchase or Is there Development board available .
I already have STM32WB55 Nucleo Pack. But I can't find reference manual or CubeMx package or examples for these microcontrollers.
void JumpToBootloader(void) { void (*SysMemBootJump)(void); volatile uint32_t addr = 0x1FFF0000; HAL_RCC_DeInit(); HAL_DeInit(); SysTick->CTRL = 0; SysTick->LOAD = 0; SysTick->VAL = 0; __disable_irq(); __...
It's not listed on the "Packages Manager" and when I try adding it manually from zip file downloaded from the I-CUBE-LRWAN website (version 1.2.1) I get an error saying "This Package version is not managed on this version of of STM32CubeMX".
I am using a modified version of the ping-pong example. I am able to go to sleep and wake up on button press in order to send a TX message to another B-L072 receiver. My issue is when I put the receiver to sleep I am unable to make it wake up from ...
I am using Nucleo-64 LR072Z board with GPS module(GPS Module TTL UART) by rhydolabz.With using HAL libraries i can send the NMEA PMTK commands but while receiving the Data from GPS module HAL_UART_Receive function gives HAL_ERROR....please help me t...
HelloI m Electronics engineer in Turkey.I m designing bluetooth controlled led lamb. It must be controlled by phone ios and android. And it must connect each other.Would you advise me a module and application
Hi,I use the b-l072z-lrwan1 to make lora advertisment and it's work.I use the project AT_slave or END_Node.But i want to use the second uart USART1 and nothing work in the environment.If i just change the file B-L072Z-LRWAN1\Applications\LoRa\End_Nod...