STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Resolved! Can't download STSW-BNRG2N-V320 Package

Hello, I tried many times(with different browsers) to download the package to use it with the BLE-NRG2-Module(Evaluation-Board). The Page keeps looping between login and the main-page with no success.     Thank you Amir

AElgh by Associate III
  • 2268 Views
  • 3 replies
  • 0 kudos

Resolved! UTIL_SEQ_WaitEvt and HW timer

Hi I have a infinite loop that wait an event set in a gpio interrupt bywhile(1){UTIL_SEQ_WaitEvt()...}It works.Now, I want have a timer after this so, if the interrupt doen't fire for some second, I want to exec a callback function.I added after UTIL...

AColl.7 by Associate II
  • 1962 Views
  • 2 replies
  • 0 kudos

BLE_AT_Server application for STM32WB5MM module

Hi,I am looking for the BLE AT server example created using a recent STM32CubeIDE release (1.14.0+) for the STM32WB5MM module. I can't find it.The most similar project I found was to open in STM32CubeIDE 1.14.1 the AT server example provided for the ...

JMarq.1 by Associate III
  • 2015 Views
  • 2 replies
  • 0 kudos

Resolved! Wifi on B-U585I-IOT2A using SPI

Hello, I'm working on the Wifi on the board B-U585I-IOT2A. I'd like to connect 2 modules, including the microcontroller, to the same wifi so that they can communicate with each other.I've made some research about Wifi MXCHIP EMW3080 and example HTTP_...

AI_STM by Associate II
  • 3211 Views
  • 3 replies
  • 2 kudos

Resolved! STM32WB55RE

Hello,   I am using STM32WB55RE (MCU) in my custom HW. For testing the HW I have flashed BLE_HeartRateFreeRTOS example firmware. "..\..\STM32Cube_FW_WB_V1.16.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRateFreeRTOS"  I am getting the ad...

Resolved! STM32CubeWL: new release planned?

STM32CubeWL = "STM32Cube MCU Package for STM32WL series", currently version 1.3.0.Is there a new release planned?Background: We are using version 1.3.0. We have issues with an application based on LoRaWAN_End_Node_FreeRTOS. We suspect the FreeRTOS in...

JBive.1 by Associate III
  • 1543 Views
  • 1 replies
  • 0 kudos

Resolved! __HAL_RCC_LSEDRIVE_CONFIG() WB55 vs WB5MMG

I see a higher drive in the WB55MMG #ifdef WB55__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);#else WB5MMG__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_MEDIUMHIGH);#endif // MIGO_BORAD would like to preserve as much power as possible, what are the consequences...

DS.4 by Senior II
  • 2067 Views
  • 3 replies
  • 0 kudos