STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 RTC with battery backup

Hello everyone, I hope you are well.I'm working with the STM32WB55. I'm having difficulty getting RTC to work correctly.The VBat is always powered by 3v3, I have an on/off switch that only removes the power from the VDD, however, when I turn it off a...

ffjunq by Associate III
  • 3124 Views
  • 4 replies
  • 0 kudos

Amazon Sidewalk Support for STM32WL

Currently, there isn't any support for Amazon Sidewalk for the STM32WL. The only supported vendors are Nordic, Silicon Labs, Texas Instruments, and Quectel. Reading through the AWS Sidewalk spec, it seems like the chip could support it in CSS and FSK...

DWalk.3 by Associate III
  • 2853 Views
  • 3 replies
  • 3 kudos

Resolved! RTC is not incremented with a voltage Vbat below 0.6V

Hello,we use an STM32WB55 with an RTC backup via a super capa.when the Vbat voltage drops below 0.6V, the RTC registers are no longer incremented.if the board reboots at this point, we have a datetime offset.is it possible to detect this problem when...

Resolved! Using OLED and gyroscope of STM32WB5MM-DK

I am using STMcube ide for developing applications with STM32WB5MM-DK. I will be trying to use the OLED display and gyroscope of the discovery board. I couldn't find suitable tutorial or documents for accessing. Is there any documents available for t...

Manually sending an I2C stop command.

In the manual it says that a stop command will be sent with the next byte if the CR2 stop flag is high.  Is there a way to send a stop command immediately rather than with the next byte?  I'm asking because I have a section of code where I send a sta...

Jcoll1_0-1707080808253.png
Jcoll.1 by Associate III
  • 5325 Views
  • 6 replies
  • 0 kudos

Resolved! STM32L0 LoRaWAN -> Whenever I set date and time to internal RTC, my system will crash.

Hello,I'm currently working with an STM32 microcontroller, and I'm facing a challenge related to the internal Real-Time Clock (RTC). Specifically, whenever I attempt to set the date and time using the internal RTC, my system crashes. I've reviewed th...

Resolved! Multitasking radio and sensor reading task.

Hello, I am currently building an application for the STM32WL. Two processes need to run simultaneously, the first is offline, and just reads data from a sensor and stores it in SD memory. The second is sending a LoRaWAN up-link message every 10 minu...

jflaxman by Associate II
  • 4544 Views
  • 3 replies
  • 0 kudos

Fail to find my nucleo-WL55JC2 in the BLE Sensor App

Hello everyone, So I'm following the tutorial here https://www.st.com/en/embedded-software/x-cube-ble2.html to try a BLE connection from the nucleo-WL55JC2 connected to the BLE expansion board X-NUCLEO-BNRG2A1. I followed the tutorial and run the pro...

LearnCORE by Associate II
  • 3922 Views
  • 4 replies
  • 0 kudos