STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! UNIX time

Is there a new "standard" way to handle time other than the original UNIX time was mentioned in AN5406 - Rev 7 - How to build a LoRa® application with STM32CubeWL, which will overflow in year 2038?TIA

David_ by Senior
  • 2350 Views
  • 3 replies
  • 2 kudos

Wireless Copro binaries

Hi,I´m just starting with Matter over Thread (with the Lighting-App from github).I´m  a little bit confused which binary is for which purpose, because the file various file names:- BLE_Thread_dynamic / static (from STM32Cube_FW_WB_V1.19.0)- Thread_xx...

AWack by Senior
  • 1302 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55 wireless binaries Source

Is the source code used to generate the Wireless binaries for STM32WB55 co-processor accessible?I am looking for the source code of stm32wb5x_BLE_xxxxx.bin.Regards,Bastien

ED_BLS by Associate
  • 1047 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeWL vs STM32Cube_FW_WL

Is STM32CubeWL the current HAL for use with STM32WL5JC Lora MCU?   version 1.3.0 https://www.st.com/en/embedded-software/stm32cubewl.htmlIs the STM32Cube_FW_WL outdated and replaced by the above?TIA

David_ by Senior
  • 1379 Views
  • 1 replies
  • 1 kudos

Resolved! Li ion cell charging and protection circuit for STM32WLE5JC

(mildly off topic) To power the STM32WL5EJC, we need to make a custom board incorporating the charging and protection circuit since 30mAh Li ion cell does not have build-in protection board. Appreciate circuit diagram, for or similar to, the popular ...

03962A_Charger_TP4056.jpg
David_ by Senior
  • 1810 Views
  • 4 replies
  • 2 kudos

Resolved! Fail to download from github using git for STM32CubeWL

At this link,  using "Windows PowerShell" on Windows 11,  https://github.com/STMicroelectronics/STM32CubeWLusing method 4, failed.git clone --recursive --depth 1 --branch v1.3.0 https://github.com/STMicroelectronics/STM32CubeWL.gitCloning into 'STM32...

David__0-1712679646183.png
David_ by Senior
  • 3049 Views
  • 4 replies
  • 1 kudos

📡 Help Needed: STM32WB10CCU5 OTA Handler

Hi all,I hope you're doing well. I'm working on a project with the STM32WB10CCU5 microcontroller and could use some help with setting up an OTA (Over-The-Air) update handler. I've searched through docs and examples but can't find a fit. Most resource...

SMazu.3 by Associate III
  • 1026 Views
  • 0 replies
  • 0 kudos

Resolved! Memory issue while using "STM32WB1MMC"

During compilation with IAR, I ran into an error. Please refer to the picture below. Upon checking the source size via the map file, it appears as follows: After examining the RAM size, it seems that the capacity of SRAM1 is less than 12K. I believe ...

KWOOJ_0-1710921360010.png KWOOJ_1-1710921515091.png KWOOJ_2-1710921563171.png
KWOOJ by Associate III
  • 1374 Views
  • 1 replies
  • 0 kudos