User Activity

Hello ST experts,I hope this message finds you well!I am writing to request your support for a project involving the Nucleo-WL55JC. I have successfully communicated between two Nucleo boards using RF communication with the SUBGHZ protocol (not LoRa)....
 Hello ST experts,I am a beginner with the STM32WL series and need some support.So first I started with the STM32F407VG disc1 and I tried to communicate two boards of it using a SI4432 module and I didn't succeed, I tried something else and I bought ...
Hi ST experts.I used the pingpong sample code with the tutorial I have found in the TechForum: Link of the tutorial in order to establish the radio frequency communication between two Nucleo-WL55JC2 boards and it works.  And then I tried to communica...
I'm currently working on a project based on transmitting RF.The objective of the project is to develop a system which is able to communicate with another device based on RF transmission.The system has to be able to provide RF communication at a frequ...
Hi guys!I'm currently in charge of a project based on the RF transaction. My project is based to develop a system that have the ability to communicate with the RF transceiver, first I chose the AS4432SMD developed with the SI4432 transceiver and I tr...
Kudos from
Kudos given to