STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Choosing ADC Reference Voltage

Hello, My problem is that I have a custom STM32WB55RG board and I want to use ADC reference voltage as 1V or as close as possible to 1 V. My questions are:1- In datasheet, it states that "If VDDA> 2V, it should be 2<Vref<VDDA and if VDDA<2V, Vref sho...

Yusuf by Associate III
  • 3573 Views
  • 5 replies
  • 0 kudos

Resolved! STM32WB5MMGH6TR and EN 300328

Hi, We are using STM32WB5MMGH6TR pre-certified module on our product. Our certification parnter insisted that we should perform tests under EN300 328 even though the module is RF tested and there is no RF design on the product side.  We tried to use ...

test fail.png

Problem on Shundown mode in STM32WB

Hello All,                 I am using STM32WB5MMG for BLE  Application,  I want to  initailly mcu is stop mode or sleep mode,when external interrupt (switch)  is triggered  its wakeup from low power mode.After wake up  re-installize the System Clock ...

Kavinraj by Associate III
  • 1494 Views
  • 1 replies
  • 0 kudos

Resolved! Requesting Support for Nucleo-WL55JC Project

Hello ST experts,I hope this message finds you well!I am writing to request your support for a project involving the Nucleo-WL55JC. I have successfully communicated between two Nucleo boards using RF communication with the SUBGHZ protocol (not LoRa)....

Zayoud_0-1717417199023.png
Zayoud by Associate III
  • 7224 Views
  • 14 replies
  • 4 kudos

error in generate code for stm32WBA54 with MX tools

For your informationSizeof is used in place of strlen and my coordinator receive a \0x00 at the end of the string !!when i generate code with MX generation tools, in function : in red old code in green new code void APP_ZIGBEE_ConfigBasicServer(void)...