STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

The program is stuck in SHCI_C2_BLE_Init

When I was debugging, I found that the program got stuck in SHCI_C2_BLE_Init, and it neither returned success nor failure.What is the reason for this? I correctly burned FUS and protocol stack when I confirmed, and the version also corresponds. 

YUNLEI_0-1718075987837.png
YUNLEI by Associate II
  • 1212 Views
  • 1 replies
  • 0 kudos

Resolved! Zigbee End Device Loosing Connection in Sleepy Mode

Hey,im developing a zigbee sleepy end device. The device is supposed to periodically send sensor values (max length of 512bytes) read via I2C to the coordinator using the custom cluster. I use the HW_TS to trigger the sensor readings and sending the ...

Errors.JPG nvic.JPG
user5 by Associate II
  • 5815 Views
  • 10 replies
  • 0 kudos

Resolved! NUCLEO-F746ZG

Where can I find the st-nucleo-lora-gw-atfw-v2.0.2.bin for the NUCLEO-F746ZG board 

snsanjay by Associate
  • 1416 Views
  • 1 replies
  • 1 kudos

Board resets systematically from standby mode

Hello,I would like to reach the lowest consumption as possible. I am programming an end node which sends data through TTN. My project is based on the LoRaWAN End Node example with the LoRaWAN middleware. My fimrware works like that :at boot, the boar...

nogema by Associate II
  • 6486 Views
  • 10 replies
  • 0 kudos

Resolved! STM32WL5MOC no transmit

Hello,I have developed a breakout board for the STM32WL5MOC for development purposes and it uses both rf switches and the wiring is identical to the B-WL5M-SUBG1 evaluation board.Running the B-WL5M-SUBG1 sample application SubGhz_Phy on my board and ...

communication with sensor: scd41-d-r2

Good evening, I ask for help regarding the communication between stm32wb5mmght6tr and the scd41-d-r2 sensor. I connected the sensor to pins PC0 (SCL) and PC1 (SDA) and powered the sensor but after loading the code I attach, the i2c communication give...

image.png
Matteo1 by Associate
  • 1707 Views
  • 0 replies
  • 0 kudos