cancel
Showing results for 
Search instead for 
Did you mean: 

Link Range of SPSGRF running 868MHz in stm32 B-L475E-IOT01A

HariCharanR
Associate

What is the maximum Link Range in the SPSGRF running 868MHz in stm32 B-L475E-IOT01A2 Board ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @HariCharanR and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The SPRGRF maximum link range depends on various factor such as the output power, the environmental conditions and the use case you are working on. With the best configurations, you can even have a link range of several hundred meters. 

Best Regards.

STTwo-32

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.