Hello,I made 2 project about client and server using stm32wb1mmc product. > server project is using "custom p2p server"It works well but I want to improve usability. 1. How to reduce scan time for connect client to server? > I quote it from examples...
HelloI've been recommended the product by the ARROW sales manager, but I'm not getting any documentation or technical help. I'm new to st product and ble.Below are the features I want.1. If you don't do anything for a certain period of time, you will...
Hi,It's first time using st product to me.according to that's UM, i thought that connect CN11 to PC it work debugging.but it wasn't and showed warning message "No ST-LINK detected! Please connect ST-LINK and restart the debug session"ST-LINK isn't in...
Hi,I'm study bootloader.using STM32F401RE at windows10.when i download bin file, below picture error occured.i attach my bootloader and application.best,Kim
Hi,I study about bootloader.And I get example files 'STM32F4 IAP' but it doesn't apply STM32 IDE.Can not build & debug.How can i get some STM32F401RE Bootloader example?
Hi Mattias,Of course, Yes I am.This problem solved by my head. Just change code like below picture.But I am wondering how this change solved the problem.Best regards,
Hello Dario CUCCHI.Thanks for reply.I have additional question.Page 19 in datasheet, R_EN and C_EN's value are 39KΩ and 10nF.In the graph that is the basis of the recommended value, the value of V is 3.3V.Also in page 18, FAULT and EN pins in MUC a...