STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Resolved! CubeMx HeartRate Needs Not Avail Cube_FW_V1.20.0

HelloI have CubeMx v6.11.1.Am trying to start a BLE_HeartRate project targeting P-Nucleo-WB55-Nucleo, and CubeMx is needing STM32Cube_FW_WB_V1.20.0This is not available at the ST website. Can you send me this or tell me how to create this project usi...

GRama.2 by Associate III
  • 4247 Views
  • 6 replies
  • 0 kudos

Resolved! STM32WL33KB 2.4GHz frequency band support

The datasheet of STM32WL33KB states that the frequency bands 159-185 MHz, 413-479 MHz, 826-958 MHz are supported.However, the website mentions that "For greater flexibility, it supports wide frequency bands from 100 MHz – 2.4 GHz". Can I get some cla...

image.png leahjoseph_1-1718883117832.png

Resolved! Hardware/fuse disabling OTA updates for security?

Hi All!We have a requirement to disable OTA updates either via hardware or by settings a fuse, this is due to the need for a low-maintaince, low-complexity, high-security method to prevent updates to those without physical access to the device.Is the...

Resolved! Problem to build any project of repo STM32CubeWB

Can anyone tell me how to do it without wasting days to simply compile a project from the repo:https://github.com/STMicroelectronics/STM32CubeWBalthough if I import any ìxample from stm32cubeide when I compile it tells me that there are missing libra...

Resolved! BLE re-pairing is not possible.

Hello. I am developing a BLE HID device using the STM32CubeWB MCU Firmware Package, but when I try pairing => disconnect => pairing, pairing fails.   I have an implementation like this, is there a problem?We have the following data in adv_data, whic...

ELEHM_1-1718778784865.png
ELEHM by Associate II
  • 1919 Views
  • 2 replies
  • 1 kudos

Resolved! STM32WB55CG (USB dongle)

Hello, where I can find info about STM32WB55CG (USB dongle) usage description and what Blue Tooth USB dongle can be used with STM32WB5MMG module ?

GS2 by Senior II
  • 4303 Views
  • 9 replies
  • 1 kudos

STM32WL55 uart error with RF

Hi I am testing with STM32WL55CCU6.When I use only uart1, uart1 works well.but when I use uart1 and RF(LoRa) send, MCU does not work.​I coded that MCU transmit some message using uart to terminal per second.MCU continues to work fine.but I added some...