STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! JTAG interface available for the STM32WB5MMDK ?

Good afternoon, I am currently working with the STM32WB5MMDK. Upon verifying the documentations, I couldn't find any mention of a JTAG interface for debugging purposes. I wanted to know if the JTAG pins can be used for programming and debugging as SW...

Nour by Associate III
  • 3510 Views
  • 6 replies
  • 2 kudos

Infinite loop into Sequencer (UTIL_SEQ_WaitEvt)

Hello,I am always getting stucked into an infinite loop when calling the sequencer UTIL_SEQ_WaitEvt().When digging deeper, I've seen that it could be a race condition as it doesn't always stop at the same function (sometimes PreIdle, sometimes PostId...

APOIR.1 by Associate II
  • 1594 Views
  • 1 replies
  • 0 kudos

Matching impedance between WB55 and MLPF-WB-01D3

I'm having a bit of an issue understanding what's going on with the impedance matching between the WB55-48QFN and the MLPF-WB-01D3 (made specifically for the WBxx family). Per another post in the community, and the WB55 documentation, I now know that...

Tulkas by Associate
  • 2145 Views
  • 1 replies
  • 0 kudos

1.8V VDDA-Vref Voltage

Hello, I have a custom STM32WB55 board and for custom purposes, I want to use VDDA=1.8 V and Vref=1.8 V from same Reference IC. According to datasheet, I can decrease VDDA from 3.3 V to as low as 1.62 V but I just wanted to make sure that it won't ca...

Makif by Associate
  • 1214 Views
  • 1 replies
  • 0 kudos

Modify a project base ble_pheripal_lite

When I create my basic project   choose from ST32CUNE ide the example  ble_pheripal_lite all is ok .The problems arrive when I want add  for example a new periperal how ADC .... How can add in the driver the adc the stm32wbxx_hal_adc.c!!!!Thanks

battellino_0-1719209291918.png