NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am working on a custom board with the STM32WB55 microcontroller.The BLE_Ota and Main APP software are functioning properly.However, when the microcontroller jump to from Ble_OTA to the Main APP, the advertising stops.When I remove the BLE_Ota softw...
Hello, I am developing a temperature measurement system which consists of a coordinator and multiple sleepy end devices. On the Coordinator Side ZbZclAttrReportConfigReq is used to set end devices reporting interval. To ensure the sleepy end-devices ...
Hi, I am facing issues with upgrading fp-atr-astra1 version 0.1.2 to the latest firmware update, which is 2.0.1. What I do is I directly upgrade the firmware using the Android app "The Ble Sensor." I upgraded by selecting a file called "STMicroelectr...
I currently have a product that uses the STM32WB55 microcontroller, and we have developed a phone app that has all of the user interface to the product, and it also performs OTA updates.I'm working on a new product and I'm considering the STM32WB0 se...
Greetings I have a STM32WB55 P-Nucleo board, with the STM322B55 dongle. I am trying to flash the beacon project onto the nucleo board. I have downloaded the STM32WB repo from the github linkI unzipped the file and selected the .project from the follo...
Hi all,I'm new to ST and was a Nordic device users.Few questions before jumping into ST.My need is to build a radio based remote control (not BLE), that means a transceiver for TX on one side and RX on the other one.Also mandatory: Digital and Analog...
I noticed that the STM product P-NUCLEO-LRWAN1 is marked as obsolete. This kit includes the Nucleo-L073RZ and the SX1272MB2xAS LoRa® extension board. However, when searching for these components individually, both are still listed as active.This situ...
Hello Everyone,I hope you are doing well.I am currently testing the Sigfox_AT_Slave example from the STM32WL repository. My end device is configured with an ID, PAC, and Key for the South Africa region (RC = 1), as provided by the Sigfox build team. ...
Hello, I am working on a BLE project with the B-WB1M-WPAN1 development board.For connection and testing, I am using the ST BLE Toolbox.For connection between the central (my phone) and peripheral (STM32WB), the pass key option is enabled, with IO cap...
Hi, there our new product needs STM32WB5MMG module to establish BLE and Zigbee link, also want to support BLE mesh and Zigbee mesh, so my question is do we have a sample project which can help us to know how to build these wireless feature? we hope...