cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-Matter unable to add to CubeIDE 1.14.1

Alec Davis 2021
Associate III

After downloading en.x-cube-matter-v1-0-3.zip and attempting to install from a local folder, as CubeIDE 1.14.1 nor 1.15.1 have it listed as a package yet.

It asks for the .zip or .pack file, shortly after selecting the zip file I get the message as in the snip below.

Tried on 3 different Windows 11 pro 64bit machines, from a Core i5 to a Core i9 13900.

 

AlecDavis2021_0-1716412604221.png

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Alec Davis 2021 

The X-Cube-Matter is not yet supported on the Current version but it will be supported ASAP. For Now, you have to start from one of the existing examples and adapt it to your needs.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @Alec Davis 2021 

The X-Cube-Matter is not yet supported on the Current version but it will be supported ASAP. For Now, you have to start from one of the existing examples and adapt it to your needs.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.