STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Batch of Dead STMs received?

(Referencing forum post: STM32WL + ST-Link = Target no device found (Custom Board))My team recently ordered a set of STM32WLE5CCU6 from Digikey for a LoRa Radio project of ours. We got the PCBs manufactured from a local vendor and began assembling ou...

Resolved! Can't build STM32WL FUOTA example with STM32CubeIDE

Hi,i'm trying to run example of LoRaWAN FUOTA firmware, but build attempt ends with fail. It looks like running postbuld.sh script fails, but it only gives an information about 4 errors without any comment.After run ./build.bat I got following logs:#...

meloon by Associate II
  • 3851 Views
  • 6 replies
  • 0 kudos

Resolved! Working with aci_hal_tone_start WB55

Hi, I am trying to check the oscillator tuning of our boards and did some reference testing with a WB55 Nucleo. using aci_hal_tone_start. Using 0,0 I do get an output near 2.402GHz, but not quite were I would expect it. The header says the following:...

OliM by Senior II
  • 1201 Views
  • 1 replies
  • 2 kudos

STM32WL55 doesn't work with 1.8V

Hi,I am working on a LoRa application with the STM32WL5MOC module which features the STM32WL55JC microcontroller. According to the datasheet, this module is compatible with a voltage level as low as 1.8V.I am using the STM32CubeWL MCU Package for the...

SMav by Associate II
  • 2552 Views
  • 6 replies
  • 2 kudos

OTA Firmware Update Bootloader

I'm working with an STM32WB09KE microcontroller and have implemented a bootloader to handle firmware updates downloaded via Bluetooth. The bootloader copies the downloaded firmware into the active application slot, and it works well for simple applic...

Emueller by Associate II
  • 4102 Views
  • 3 replies
  • 0 kudos

STM32WB09 - No read event is generated

Hello. Im having issues generating an event when pressing read on my smartphone, on my CHAR_PROP_READ characteristic in my BLE service. I enabled the "GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP", which should notify when a read request of any type i...

s215477 by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos