STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 223 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! Middleware for stm32wba52cgu6 microcontroller

I am using smt32wba52cgu6 MCU in my project. In this project i want to use SD card module but since the module has no FAFTS middleware in STM32Cube Mx as well as in STM32cube IDE. I am using the libraries available in the git hub for fafts (https://g...

Shaku by Associate II
  • 1377 Views
  • 2 replies
  • 1 kudos

How to increase BLE payload size

Hi,I am using the example ble_p2pServer_ota with STm32WBA55. I would send a packet between a client and a server with more than 20 bytes.Here is part of the code from p2p_server.c:When i debug the code, the value of Attr_Data_Length is correct until ...

ledi7 by Associate III
  • 1302 Views
  • 1 replies
  • 0 kudos

STM32WL33 Bootloader documentation.

Hi.I am looking for some info relating to the factory bootloader in the STM32WL33. In a nutshell, I dont need it nor want it. My application will require a custom bootloader that will read program from EEPROM over SPI.I have discovered from a previou...

CEagl.1 by Associate III
  • 1411 Views
  • 1 replies
  • 0 kudos

Wio E5 CubeMX library include issues

I am using Wio E5 board for a LoRawan project and running the project FreeRTOS LoRa Wio E5  in STM32CubeIDE. When building the project as it is without changing anything in CubeMX it works fine. I could change the EUI values, region, etc.. in the res...

user_01 by Associate III
  • 5797 Views
  • 3 replies
  • 0 kudos

Resolved! Cannot Download BLE_HeartRate program into WB55rg

Hello there,I'm trying to execute the BLE_HeartRate Service example on WB55rg Nucleo board. Initially I successfully run the code.Later I'm trying to download the same code again BUT I'm getting following message repeatedly in the CONSOLE:Download ve...

OS_Er by Associate II
  • 948 Views
  • 1 replies
  • 0 kudos

WB55 BLE client custom board

Hello.I have my custom PCB with STM32WB55CEU. This board is tested so I m able to connect and sending data beetween "my PCB" and Smartphone.Now I have new goal. The goal is to start scan process for nearby devices. I would like to hit breakpoint whic...

Bez tytułu (1).png Bez tytułu.png

STM32WL33 QSPI VS SPI

Hi I am hoping someone might be able to help me with some calculations.I am assessing the STM32WL33 for use in a product.One of the peripherals will be an EEPROM, an M95P32.The EEPROM supports Dual/Quad Output (Read) However the STM32 does not appear...

CEagl.1 by Associate III
  • 1426 Views
  • 1 replies
  • 0 kudos

Resolved! aci_gatt_add_service() returns BLE_STATUS_OUT_OF_MEMORY

I am adding services to an existing WB55 BLE project with a small number of services.As I increase the number of services, aci_gatt_add_service() eventually returns 0x98, BLE_STATUS_OUT_OF_MEMORY. (I note that 0x98 is not shown as a valid return valu...

TWood.4 by Associate III
  • 1311 Views
  • 1 replies
  • 0 kudos