2023-02-27 5:53 AM
I'm trying to use Bluetooth on the Nucleo WB55RG board to make them communicate with each other. I find on internet a solution using micropython and Bluetooth import (this link of Solution: stm32python.gitlab.io/). However, when I activate the module, an ETIMEDOUT appears, so I try to increase the NIMBLE_STARTUP_TIMEOUT (up to 20s) but nothing changes. Not finding a solution to my problem I turn to you to try to find a solution.
I tried to update the firmware. Result: Memory erased but firmware crashed in the download. I still managed to put the compiled firmware back as shown on the previous git. By a happy miracle, the error changed to
tl_ble_wait_resp: timeout. Does anyone know why the bluetooth doesn't work?
Thanking you in advance.
2023-02-28 6:44 AM
Hello @ropouillard and welcome to ST Community
Thank you for posting!
This GitLab is still under development, and there are ongoing updates on several applications.
However, you can use the firmware 1.19.1 (from downloads) and test this example (it is now available only in French, hope it's not a problem for you!)
but make sure to erase the memory with STM32CubeProgrammer first
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-01 12:59 AM
Hello @Sarra.S
Thank you for answers.
To my first test I followed your example (the french is not a problem). And my first error was
OSError: [Errno 110] ETIMEDOUT But for that I had stupidly followed the instructions (so by getting the code on git and not the 1.19 stable present on the site).
However by using 1.19.1 firmware this error appeared:
tl_ble_wait_resp: timeout. (like explain in my question).
Thank you!
2024-07-03 2:04 PM
Dear all,
I am also trying the same, but I have few question.
Do I need to still flash the firmware for the co processor while trying the micropython, or the micropython is having the firmware built for the coprocessor( BLE ).
2nd part, I was tryign an exampel from the following link
https://stm32python.gitlab.io/fr/docs/Micropython/BLE/BLEGAP
But everytime I am getting the following error.
Traceback (most recent call last):
File "<stdin>", line 39, in <module>
File "<stdin>", line 24, in __init__
OSError: [Errno 110] ETIMEDOUT
Please suggest how can I fix it.