STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

framebuffer size +3 ???

I am working on a project with TouchGFX on STM32H7 with 240x320 RGB Display. Framebuffer is in internal RAM.I calculated the RGB565 framebuffer size to 240x320x2 bytes and allocated this amount in the linker file with "TouchGFX_Framebuffer" atttribut...

WSchr.1 by Associate II
  • 1095 Views
  • 1 replies
  • 0 kudos

Using TouchGFX to draw more than 5 interfaces on STM32F429, the switch happens to be stuck or even unresponsive, now I don't know how to analyze the problem.

Hardware :STM32F429 + LCD_1024*600Software: FreeRTOS + TouchGFX The system consists of two tasks, one LED task and one TouchGFX task.TouchGFX task mainly do a few simple interface, no complex interface drawing, the image resources are stored in ex...

TouchGFX Modal �?서 키를 받�?�수 있나요?

안녕하세요. ​Modal�?� �?�운 �?태�?서 터치스�?�린 입력�?� 받아서 사�?�지게 하고 싶습니다.버튼 키를 사용하지 않고 스�?�린 아무곳�?� 터치 해�?� 받�?�수 있는 방법�?� 있나요?​​답변 부�?드리겠습니다.�?사 합니다.​

Phyo .1 by Associate II
  • 6205 Views
  • 3 replies
  • 0 kudos
GAuye by Associate III
  • 2482 Views
  • 5 replies
  • 0 kudos

TouchGFX / Hardware integration tutorials

Hi thereI have been experimenting and creating simple TouchGFX GUI applications on STM32 touch screen dev kit.Is there a simple start guide to creating as simple touchGFX GUI and controlling an LED on the STM32F429i Disco board? I tried some online e...

LAlna.1 by Associate II
  • 9006 Views
  • 19 replies
  • 0 kudos

Help with using a custom font in STemWin.

Hi all. I am currently working on a project using my STM3220G board with a 3.2 " TFT and STemWin. I have made a custom font with only the hebrew alphabet in the font. The font .c file is below: /*******************************************************...

defacato by Associate II
  • 1536 Views
  • 0 replies
  • 0 kudos