2020-06-04 6:14 AM
Hello,
I am working with a STM32L4R9 and I am trying to extract a (STemWin) JPG decoded image to a BMP buffer (in external RAM).
First of all :
- I am using a 400x400 pixels screen, GFXMMU is initialized, 16bpp color depth.
- I can display a jpeg image using 'GUI_JPEG_Draw'.
- Other STemWin functions seems to work correctly as well (GUI_BMP_Draw, etc.).
* First case scenario
- I print the jpeg image to my display using 'GUI_JPEG_Draw'.
- Then, when I try to get the content of what it is displayed using 'GUI_BMP_Serialize', I only received blank data in the serialization callback (the header seems to be correct, but all other bytes are 0).
Is there something to do before using 'GUI_BMP_Serialize' ? Why all the bytes received are blank ?
* Second case scenario
- I move STemWin dedicated memory to external RAM to be able to create a memory device.
- I create a memory device (no error returned).
- I select the newly created memory device.
- I use 'GUI_JPEG_Draw' to decode JPEG into the memory device.
Multiple issues in this case :
- Nothing is displayed when I try to display the content of my memory device (using 'GUI_MEMDEV_CopyToLCD').
- When I check the content of the memory device (using 'GUI_MEMDEV_GetDataPtr' to get BMP address), every bytes are set to 0.
- When I try to get the content of the memory devic (using 'GUI_BMP_Serialize'), all data received are 0.
Am I missing something ? What am I doing wrong ?
Thanks in advance for your response.
Regards,
Jon.