Skip to main content
SK S.1
Associate III
June 4, 2020
Question

Can anyone suggest me 8" to 10" TFT LCD + Capacitive Touch screen with MIPI DSI interface which can be directly connected to STM32F469I-Discovery Board?

  • June 4, 2020
  • 11 replies
  • 4726 views

Hi Guys,

I want to connect 8" to 10" TFT LCD + Capacitive Touch Screen display with MIPI DSI interface to STM32F469I-Discovery just by removing the existing 4" TFT LCD. I had searched in the internet and I didn't get any TFT LCD CTP with MIPI DSI interface which can be directly connect to STM32F469I-Discovery board. STM32F469I-Discovery board uses 25 pin connector (CN10) for LCD and 6 pin connector (CN2) for Capacitive Touch screen.

Can anyone suggest me 8" to 10" TFT LCD + Capacitive Touch screen with MIPI DSI interface which can be directly connected to STM32F469I-Discovery Board?

With Regards

SUNIL K S

Ace Designers Ltd

This topic has been closed for replies.

11 replies

SKacp.1
Associate
June 4, 2020

Hi,

Please try to find products from Powertip. For example: PH720128T003-ZBC02 - 7" 720x1280 with MIPI DSI. They also offer 10" TFT LCD but I do not see on the website. Please ask the distributor. https://www.powertip.com.tw/TFT_Touch_Panels.html#prhome

SK S.1
SK S.1Author
Associate III
June 4, 2020

​Thanks a lot for the help.

With Regards

SUNIL K S

SKacp.1
Associate
June 5, 2020

Hi,

I have ordered TFT LCD  PH720128T003-ZBC02. I plan to connect with STM32MP1 (module VisionSOM-STM32MP1 company SOMLabs) https://somlabs.com/product/visionsom-stm32mp1/. I have also plan to connect with STM32F769 or STM32H74x.