STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STemWin's simulator, color problem.

Hello,We have facing troubles with STemWin's simulator.Our embedded project creates the GUI driver like this:void LCD_X_Config(void) {   GUI_DEVICE_CreateAndLink(GUIDRV_LIN_16, GUICC_M565, 0, 0); ... }  Our simulator project create...

nicolas b by Associate III
  • 784 Views
  • 0 replies
  • 0 kudos

how to configure DCMI for embedded sync?

I have STM32H7 DCMI + TVP5150 I want to get the frame, the only result that I get is 720 pixels and no more. My main culprit is DCMI->ESCR register, could please anyone help me? I calculate SAV EAV codes, but using them I elicit no result that differ...

esukh by Associate III
  • 825 Views
  • 0 replies
  • 0 kudos

I do not enter in HSYNC interrupt DCIM STM32H743

I want to fetch video data from camera via decoder (TVP5150AM1) through DCIM.I configure decoder to output 4:2:2 8-bit YCbCr video with discrete synchronization and I do not get HSYNC interrupt, DCMI->IER |= (0x1 << 4) | (0x1 << 0);so, first time whe...

esukh by Associate III
  • 761 Views
  • 0 replies
  • 0 kudos