User Activity

Hi,I can currently only find support for STM32MP157A-DK1 and STM32MP157C-DK2 boards in u-boot.Is there a plan to support the STM32MP157F-DK2 board in the near future?Kind regards,Steinar
Hi,I am using STM32CubeProgrammer version 2.12 running on Windows 10 to connect to the STM32MP157F-DK2 board ST-LINK connector CN-11.I managed to connect and when I click "Firmware upgrade" the STLinkUpgrade 3.4.0 window opens.However, when I press "...
Hi,I am writing an external flash loader for the STM32WB55RGVx using a Macronix 64Mbit QSPI NOR Flash (MX25R6435F).I have had some success following the "MOOC - External QSPI loader how to" youtube video series by ST and the example code for memory m...
Hi,I have a custom board setup using a display connected via SPI and I've used the example code from the STM32L496G-DISCO board as a reference.My SPI display driver works correctly as I am able to send data directly to the display and show it on the ...
Hi,is there any plans to add support for MAC OSX to TouchGFX as all other ST tools seem to be multi platform? It would be greatly appreciated :smiling_face_with_smiling_eyes: Kind Regards,Steinar