User Activity

Hello,It's quite easy to manipulate the CLUT for an L8 uncompressed Bitmap but how could we find the CLUT entries when the Bitmap is compressed with either RLE or LZW methods?When looking at the .cpp generated for such an image around the extra_data ...
The SVGImage widget is a great tool but, as I understand it can only use SVG images from the SVGdatabase.I may imagine to subclass the SVGImage class and handle directly run time created lists of VGObject as it is done with the SVGdatabase.What is mi...
Hello,I started a new design based on an STM32H745XI with a 480x272 TFT screen.I have some experience with TouchGFX with a previous design on an STM32H7B3 with the same screen but this development is stucked at the TouchGFX 4.17 revision.My problem i...
I'm using my V3PWR probe for weeks now... but this morning it refuses to work. It was working yesterday evening with the same setup.When I connect to the USB-C cable, no led at all , no USB enumeration ... nothing !! I changed the cable without succe...
I'm running on Mac-OS with CubeIDE V1.12.1 (the latest at this time)When I try to connect a target using SWD with my STLINK-V3PWR probe I get the following:"No ST-Link detected" in a popup named : "ST-LINK firmware verification"If I try to upgrade th...