User Activity

HI,I'm trying use SDIO interface on STM32F469I-Discovery board ​and I'm always getting FR_DISK_ERR for the command "f_open(&myfile,myPath,FA_CREATE_ALWAYS|FA_WRITE)" Same problem is observed  with 1-bit and 4-bit SDIO mode. I have enabled "Use DMA te...
Hi,I'm using TextArea with Wildcard for displaying Text Dynamically at the rate of 300​ms on STM32F469I-Discovery board and the TextArea Flickers while updating Text at 300ms rate.I have reduced the LCD clock to 10Mhz and checked as suggested by some...
Hi Guys,I have installed STM32CubeIDE 1.3.0 on my PC which is connected to office network through LAN. Even though  STM32CubeIDE is allowed  to communicate through windows firewall I'm getting network error. One more thing is STM32CubeIDE 1.3.0 is wo...
Hi Guys,I want to connect 8" to 10" TFT LCD + Capacitive Touch Screen display with MIPI DSI interface to STM32F469I-Discovery just by removing the existing 4" TFT LCD. I had searched in the internet and I didn't get any TFT LCD CTP with MIPI DSI inte...
HiI'm using STM32F746GDiscovery board. I'm using STMCubeIDE+ TouchGFX designer for GUI development.Is it possible to design a Strip Chart using TouchGFX Designer?If it is possible then please let me know the procedure.With RegardsSunil K SBangalore​
Kudos from