STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Image widget not showing properly

Hi! I'm running TouchGFX 4.21.3 on a custom board with the following hardware.STM32L452RET6QSPI W25Q128JV for storageLCD 320x172 SPI ST7789v3Everything is working fine expect that image widgets that contain alpha values are now shown properly. I'm st...

_legacyfs_online_stmicro_images_0693W00000bhelkQAA.png _legacyfs_online_stmicro_images_0693W00000bheoKQAQ.png _legacyfs_online_stmicro_images_0693W00000bheuhQAA.png
MCerv.2 by Associate II
  • 2498 Views
  • 3 replies
  • 0 kudos

"Error: failed to download Segment[1]" error occurs in the middle of downloading the STM32U5A9J-DK touchgfx DEMO project

​Hello, I just encountered "failed to download Segment[1]" error in the middle of tough gfx project downloading.Demo Board : STM32U5A9J-DKCubeProgrmmer version : 2.13.0TouchGFX version : 4.21.3Error message capture I found that toughgfx is using the ...

0693W00000bhE8DQAU.png 0693W00000bhE9pQAE.png 0693W00000bhE8IQAU.png 0693W00000bhE9aQAE.png
CARHERO by Associate III
  • 5054 Views
  • 7 replies
  • 0 kudos

TouchGFX Designer gets hanged.

If I expand screens tab on left column and there are many widgets added to a screen or there are multiple screens which requires to scroll down that list then TouchGFX Designer 4.15 gets hanged when you reach at end. Only fix then is to kill this Des...

0693W000005BuDmQAK.jpg
VShet.2 by Associate III
  • 3966 Views
  • 7 replies
  • 0 kudos

handleTickEvent in ScreenView not called - why?

Hi,I'm new with TouchGFX and working on my first project. My current problem is that I wnat to update display values from my software. I looked into several tutorials and found that when implementing the function virtual void handleTickEvent();in the...

KR51K by Associate III
  • 2983 Views
  • 2 replies
  • 0 kudos

Resolved! How to update TouchGFX Designer

I can't find the update option in TouchGFX designer software. Do I need to uninstall existing designer manually and download X-Cube-TouchGFX package again and install as a new software to update. I know that TouchGFX generator can be updated from the...

CAbey.1 by Associate II
  • 3779 Views
  • 4 replies
  • 0 kudos

Resolved! How to use touchgfx with nucleo board that is not in standard list also how to use a display controller like ili9488 or RA8875.

Hi i am very new to all stm32, i have some project that i want to move to stm32 mcus. I would like to know if i have a nucleo board that is not in the list of selections that exist in designer, or i have selected an mcu that a dev board does not exis...

Kyrpav by Associate III
  • 7690 Views
  • 24 replies
  • 0 kudos