User Activity

I have an H755 nucleo board and a riverdi 5'' rgb display.Aftersetting the ltdc ,the clock to 25mhzthe freertosnot using qspi and sdram just by using the 2 layer start address 0x20000000 and 0x20119400 for RGB888I have enabling the nvicI have crossch...
I have a STM32F755ZI nucleo board. I am trying to load and run simple project from the board selector. So creating new stm32 project and selecting the board. Then i try to load the project and while it seems to load the stlink led blinks 3 colours an...
What can i do to fix the over current problem.i have a nucleo-F767ZI board and  it seems that by trying to power on a display there is a problem with the circuit at the backlight and now i get the LD5 for the over-current always on.At this stage i do...
I am using a nucleo-f767zi to control a reverdi tft display.The project in CUBEMX ide is using freertos and there for the time base is changed from systick to TIM6.I am trying to task enable sequence for the screen but i see that i am stack in an inf...
Hi since I am very new to touchgfx this is probably a wrong or already answered question. How can someone has a user edited text line or text area with a virtual keyboard? I mean to have a text input widget that user selects it and a keyboard opens o...
Kudos from
Kudos given to