User Activity

​Hello, I just encountered "failed to download Segment[1]" error in the middle of tough gfx project downloading.Demo Board : STM32U5A9J-DKCubeProgrmmer version : 2.13.0TouchGFX version : 4.21.3Error message capture I found that toughgfx is using the ...
I bought the STM32U5A9J-DK board. I want to start digging it out by modifying the default OOB example code. But I can't find the OOB code even the binary. It would be appreciated if to provide the OOB code or binary.
I encountered an issue(v2.7.0) like the title and I fixed it just removing the "config.properties" file located in "C:\Users\Administrator\STMicroelectronics\STM32CubeProgrammer\config.properties" path.I attached my "config.properties" file which not...
Hello Cube IDE teamI am using STM32F427ZG MCU board with STM32CubeIDEBut I have trouble to generate *.bin file after building with CubeIDE.I think it support *.elf file only for now.If below command can be added into makefile, then *.bin file can be ...
Kudos from