STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Board turns black instead of displaying GUI

BACKROUND:I am using TouchGFX Designer - 4.24.0I am using the board STM32H735G-DKThis generates STM projects in STM32CubeMX V6.11.0 using STM32Cube FW_H7_V1.11.1When I am done with touchGFX I go to STM32Cube IDE to do some scripting on the behaviors ...

tmehok by Associate III
  • 1456 Views
  • 1 replies
  • 1 kudos

Resolved! how to run STM32Cube.ioc at TouchGFX project?

Hi I am luis.I'm testing TouchGFX, and I have a question.After creating an example board project with TouchGFX V4.22.1 Designer and then moving the STM32F769I_DISCO.ioc file into the STM32CubeIDE folder to set the IO, an error occurs when compiling a...

luisfynn1 by Associate III
  • 1774 Views
  • 1 replies
  • 0 kudos

Resolved! Persistent widgets between screens

I'm a touchgfx beginner but i've designed many graphic apps using other tools like lvgl. One thing my app needs is to have some common areas or widgets that work between multiple screens, like persistent widgets that always exists in all screens, is ...

Resolved! TouchGFX intelisense problems

  intellisense is not working.  the components that I can't use the intellisense feature( button, Textarea, slider, scroolist and the like...) "Screen1ViewBase.it is observed that the text colors of the implementations in the "cpp" file are also diff...

1.png 2.png 3.png
fog.1 by Associate III
  • 2227 Views
  • 3 replies
  • 4 kudos

External vs internal memory for images to store

Hi,for the application I need to develop, I need to store onboard the PCB many images and other large data. The images especially, need to update the screen background image dynamically at runtime.Because in one configuration of the system the images...

Ricko by Senior III
  • 1609 Views
  • 1 replies
  • 0 kudos

Resolved! stm32f411RE and TouchGFX

Hi, I've been trying a project focusing on GUI display on TouchGFX GFX01M1 with STM32f411RET6 NUCLEO board. I have seen videos in youtube related to TouchGFX and they say that there is a need for FMC interface and LTDC in STM32CubeIDE. But for STM32f...

viha_123 by Associate II
  • 7204 Views
  • 10 replies
  • 5 kudos

Flex Button with SVG Icon

Hi,The only way I can find to use a custom SVG as an Icon for a Flex Button is to add it to the Theme library.As a workaround I created folder in the  ..\designer\Themes\icon_theme\images\Themes directory and copied the SVG there. eg C:\TouchGFX\4.23...

codebuk by Associate III
  • 1752 Views
  • 2 replies
  • 0 kudos