STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Touchgfx without GFXMMU

I have a problem with disabling gfxmmu. I don't have a rounded display so that actually I do not need GFXMMU.I created a project by using Touchgfx Designer Templates (STM32H7S78 DK BPP). GFXMMU is activated in default. I would like to disable it. So,...

touchgfx_gfxmmu.jpeg

Resolved! NeoChrom/GPU2D registers documentation

Will this peripheral ever be documented in detail? i.e. registers, interrupts, etc.Or even a lightweight/low level library would be acceptable.We may choose STM32U5 for a product but not if we are forced to use TouchGFX for good performance. 

robvos by Associate
  • 23888 Views
  • 57 replies
  • 62 kudos

Resolved! Display the camera image using TouchGFX.

Hi ,I'm developing a product on an STM32N6 using TouchGFX. I need to display the image coming from the camera input on the product on the TouchGFX. During our tests, we were able to directly print the image from the DCMI input to the screen and it wo...

Okeskin by Associate III
  • 705 Views
  • 5 replies
  • 3 kudos