STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32H7 Cache configuration for USB HS

How do I need to configure cache validation invalidation for USB transfer to PC of continuously DMA filling buffer? Right now I have some visible errors ( I stream DCMI video via USB).

esukh by Associate III
  • 773 Views
  • 0 replies
  • 0 kudos

STemwin not work, black screen

Hello community,I have a development board with a STM32F429IGT6 processor. I connected an RGB display (without controller) to the LTDC to the board. On the board is too a 64MBIT Sdram on the FMC port. With STM32CubeMX I have been trying to brighten t...

HM?�l by Associate
  • 1629 Views
  • 1 replies
  • 0 kudos

Can DMA2D do a repeat buffer copy/fill from image ?

Hi,I have DMA2D (ChromArt) working fine for drawing images from memory to display buffer.However, to save on image storage, I would like to create single pixel image "strips" which I can repeat a number of times in X or Y.eg, for drawing a top border...

AndyJT by Associate III
  • 1613 Views
  • 2 replies
  • 0 kudos

CubeMx can't generate code for atollic with STem

HelloI'm building a first app to explore STem. I'm doing it the easy way :eval F746 and CubeMX.It appears that if I enable STem, Atollic is no more supported as IDE.(see screenshot).Is it a regular behaviour?If yes, can you communicate a reason and i...

JulienD by Senior
  • 1615 Views
  • 2 replies
  • 0 kudos

HX8238 and LTDC

Hello, I have succesfully configured several lcd screens with stm32 MCU's, but they always been "timing-friendly" and all the typical parameters were in the datasheet. Now I'm trying to use the 3,5" LCD with HX8238 using RGB 565 connection.Here is th...

SimonP by Associate II
  • 2606 Views
  • 4 replies
  • 0 kudos

Graphic application with STM32F46 discovery board

up loading the default set values in STM32f746 disco on STM32CubeMx, with following checks :1. Graphics ticked, STEmwin enabled, Guibuilder enabled2. Corrected the pixel resolutuon 480x2723. Execute Guibuilder from within StCube4. FreeRTOS5. As per S...

ZMohd.7 by Associate III
  • 1975 Views
  • 4 replies
  • 0 kudos