2025-06-22 6:52 AM - edited 2025-06-22 6:57 AM
#include "cmsis_os.h"
#include <stdio.h>
#include <stdlib.h>
#include "main.h"
#include <stdbool.h>
extern I2C_HandleTypeDef hi2c4;
uint8_t DATA, DEVICE_STATUS = 0x00, XH, XL, YH, YL;
uint16_t X_AXIS, Y_AXIS;
#define DEVICE_ADDRESS (0x38 << 1) // Shifted for STM32 HAL
uint16_t x_axis = 0, y_axis = 0;
uint8_t STATUS = 0;
void STM32TouchController::init()
{
// Initialization if needed (e.g., configure GPIO, I2C, etc.)
}
bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y)
{
static uint16_t prev_x = 0xFFFF, prev_y = 0xFFFF;
STATUS = HAL_GPIO_ReadPin(GPIOG, GPIO_PIN_2); // Touch INT pin low = active
if (STATUS == GPIO_PIN_RESET)
{
// Read X high & low
HAL_I2C_Mem_Read(&hi2c4, DEVICE_ADDRESS, 0x03, I2C_MEMADD_SIZE_8BIT, &XH, 1, 100);
HAL_I2C_Mem_Read(&hi2c4, DEVICE_ADDRESS, 0x04, I2C_MEMADD_SIZE_8BIT, &XL, 1, 100);
// Read Y high & low
HAL_I2C_Mem_Read(&hi2c4, DEVICE_ADDRESS, 0x05, I2C_MEMADD_SIZE_8BIT, &YH, 1, 100);
HAL_I2C_Mem_Read(&hi2c4, DEVICE_ADDRESS, 0x06, I2C_MEMADD_SIZE_8BIT, &YL, 1, 100);
// Combine bytes to get coordinates
uint16_t current_x = ((XH & 0x0F) << 8) | XL;
uint16_t current_y = ((YH & 0x0F) << 8) | YL;
// Store coordinates
X_AXIS = current_x;
Y_AXIS = current_y;
// Return only if the value changed
if (current_x != prev_x || current_y != prev_y)
{
prev_x = current_x;
prev_y = current_y;
x = current_x;
y = current_y;
return true;
osDelay(1000);
}
}
return false; // No touch or same value as before
}This Library runs fine but after few seconds of usage the debugger throughs the following
static void prvTaskExitError( void )
{
volatile uint32_t ulDummy = 0;
/* A function that implements a task must not exit or attempt to return to
its caller as there is nothing to return to. If a task wants to exit it
should instead call vTaskDelete( NULL ).
Artificially force an assert() to be triggered if configASSERT() is
defined, then stop here so application writers can catch the error. */
configASSERT( uxCriticalNesting == ~0UL );
portDISABLE_INTERRUPTS();
while( ulDummy == 0 )
{
/* This file calls prvTaskExitError() after the scheduler has been
started to remove a compiler warning about the function being defined
but never called. ulDummy is used purely to quieten other warnings
about code appearing after this function is called - making ulDummy
volatile makes the compiler think the function could return and
therefore not output an 'unreachable code' warning for code that appears
after it. */
}
}And if I keep my finger pressed on the GUI button, it tends to click repeatedly very quickly, and the GUI freezes after a few seconds.
2025-06-24 7:32 AM
Hello @Caan ,
I don't think this is a TouchGFX related issue, but we'll try to help you.
1- Why do you have an osDelay() inside your sampleTouch function? And if you need it, where it is placed now it's not useful.
2- Have you checked the call stack? Anything not normal in it?
3- "And if I keep my finger pressed on the GUI button, it tends to click repeatedly very quickly, and the GUI freezes after a few seconds." --> looks like an hardfault issue. Can you confirm?