MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I make BLE work on STWINKT1?

Hi,I am trying to use the BLE (SPBTLE-1S chip) on my STEVAL-STWINKT1 board. The idea was to use a project example from X-Cube-BLE2 with the following configuration :HCI_TL : BasicHCI_TL_Interface : UserBoardApplication : SampleAppI used the SPI2 to c...

KaisBo7 by Associate II
  • 1936 Views
  • 3 replies
  • 0 kudos

IIS2DLPCTR Internal LDO

I am thinking of powering the IIS2DLPCTR accelerometer VDD rail from a buck converter and wanted to understand if this part uses an internal LDO to step the VDD voltage down to power the internal MEMS block and ADC? Or does it use the supplied VDD di...

NBerr.1 by Associate II
  • 1171 Views
  • 1 replies
  • 0 kudos

SensorTile.Box PRO asks Bluetooth Code

When I connnect sensorTile.box from App.the followign msg poped ip continuously. and no fucntion work properlywhat is the reason. I upgraded the FW on FOTA  at the first connection.what is the suggestion ?Thanks!Forest  

forestxu_0-1718761080315.png
forest xu by Associate II
  • 2445 Views
  • 5 replies
  • 0 kudos

ML implementation in ISPU

Can anyone provide a documentation over integration custom ml algorithm in ISPU.If I have a machine learning model like tflite or onnx how can I deploy it in ISPU

Amith_lal by Associate III
  • 2202 Views
  • 3 replies
  • 2 kudos

ISM330DLC Low Power Mode

Trying to get the lowest power out of this device, but it seems to draw at least 900uA of current when even the accel and gyro are disabled. Any suggestions on how to get the current draw of this device lower? Here's my setup:Custom PCBnormal current...

NSmit.9 by Associate II
  • 2155 Views
  • 3 replies
  • 0 kudos

STEVAL-MKBOXPRO firmware that is compatible with ISPU dil24

I'm trying to make a demo with the ispu chip ism330is and the STEVAL-MKBOXPRO the issue is I can't find a suitable firmware for the tilebox pro that is compatible with the ispu and allows me upload the compiled UCF program into the chip. Below is a s...

benx1326 by Associate II
  • 1746 Views
  • 1 replies
  • 0 kudos

Unicleo gui not detecting IKSO1A2

Hello, I'm learning how to use stm32 hardware and how to program it and today i connect the X-NUCLEO-IKO1A2 to my board (Nucleo-GO71RB) and installed the inucleo software,  i did everythink like te st video said, but for some reason the software does...

Fxpires by Associate
  • 1601 Views
  • 2 replies
  • 0 kudos

Android HAL for LSM6DSOX sensor

Hello experts,I am using rock chip board with android 12 on it along with the sensor lsm6dsox connected on i2c2.I have added the driver and compile the Linux and then build android images.After booting I can see device is detected on i2c and probed s...

amol4394 by Associate
  • 1837 Views
  • 1 replies
  • 0 kudos