MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 FIFO Corruption

I am writing a custom linux driver module to be able to read accelerometer and gyroscope data from the LSM6DS3 FIFO in blocks.I have set the fifo watermark to 512 words, ODR for accel, gyro and FIFO both set to 416Hz. Scale 8G and 250dps. As there is...

MDSeon by Associate
  • 940 Views
  • 0 replies
  • 1 kudos

Resolved! IIS3DWB: how to detect over range

Hi,I'm using the IIS3DWB accelerometer to get triaxial waveform.I just want to know what is the best approach to detect over range.I tried to compare sample by sample in each channel with the maximum possible positive value (>32766) and the maximum n...

Palmering by Associate II
  • 2778 Views
  • 2 replies
  • 1 kudos

IIS2DLPCTR ODR Accuracy

Could you please provide information about the output data rate (ODR) for the IIS2DLPCTR accelerometer?For example, if I want an ODR of 50Hz in High Performance mode, with BW=ODR/2, how accurate is the 50Hz ODR?  Similarly, if I use the single data c...

NBerr.1 by Associate II
  • 1722 Views
  • 3 replies
  • 0 kudos

calibration of accelerometer and gyro in lsm6d

we are using LSM6DSV16x sensor with nrf5340 dk board , wea are getting values like this ACC[mg]:x:-157.50,y:-30.74,z:981.00GYRO[mdps]:x:-700.00,y:-140.00,z:420.00,please help in calbration to get accurate values of  sensor .

AlgoBuilder for IKS01A2

Hi, I understand IKS01A2 is not supported anymore in the current AlgoBuilder software versionIs it still possible to download the last AlgoBuilder version that supports this board ?I can only download the latest version from the website (no older ver...

mtzt by Associate
  • 1097 Views
  • 1 replies
  • 0 kudos

Resolved! What's best and way to calculate velocity from acceleration for IIS3DWB and what degree of accuracy should one expect with IIS3DWB accelerometer?

I am using IIS3DWB for machine condition monitoring product development project.I am using the below integration for velocity conversion as per MotionSP but unable to estimate speed RMS (not even 50% closer to the reference values).------------------...

AGosw.3 by Associate
  • 5651 Views
  • 7 replies
  • 1 kudos

Resolved! issue with NRF24L01 on STM32F07VET6 blackboard

I've been trying to interface the STM32F407VET6 with the NRF24L01 modules, however after trying multiple boards modules and library's it still fails to work. im not sure the issue is with hardware as ive tried multiple modules and the black board has...

voxe by Associate II
  • 2069 Views
  • 1 replies
  • 0 kudos

IKS02A1 and Nucleo H503RB don't work

Hi, I am curretly using a Nucleo H503RB and the IKS02A1 expansion board in order to use the ISM330DHCX.I tried several way to use via STM32Cube IDE which is my goal as i want to use C language without success to see any sign of an i2c adress with an ...

matkergo by Associate
  • 1761 Views
  • 1 replies
  • 0 kudos