MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do I program STEVAL-MKI109v3

Hi,I have STEVAL-MKI109v3 board and steval-mki186v1 sensor. I need some source code or library code which I can use to write a application which meets my requirements. And I also want to know which IDE I should be using to write the application so th...

AV B.1 by Associate II
  • 2746 Views
  • 4 replies
  • 0 kudos

IIS3DWB SDO behaviour on multi-slave SPI bus (will it work?)

Hi All,We are implementing a custom PCB which includes an ISS3DWB which sits alongside an EEPROM chip on the same SPI bus. The bus master is a STM32F405. The design will has separate CS pins for each device, chances are the EEPROM will only be commun...

IBoddy by Associate
  • 908 Views
  • 1 replies
  • 0 kudos

lsm6dsox datasheet missing informations

Hi there,After playing around with basic examples for the lsm6dsox sensor i am trying to fine tune its functionality to my exact needs. However the datasheet seems to lack information on these:#1: Does writing the SW_RESET bit of CTRL3_C register res...

RDyla.1 by Associate
  • 1036 Views
  • 0 replies
  • 0 kudos

LSM6DS3 FIFO Corruption

I am writing a custom linux driver module to be able to read accelerometer and gyroscope data from the LSM6DS3 FIFO in blocks.I have set the fifo watermark to 512 words, ODR for accel, gyro and FIFO both set to 416Hz. Scale 8G and 250dps. As there is...

MDSeon by Associate
  • 941 Views
  • 0 replies
  • 1 kudos

Resolved! IIS3DWB: how to detect over range

Hi,I'm using the IIS3DWB accelerometer to get triaxial waveform.I just want to know what is the best approach to detect over range.I tried to compare sample by sample in each channel with the maximum possible positive value (>32766) and the maximum n...

Palmering by Associate II
  • 2780 Views
  • 2 replies
  • 1 kudos

IIS2DLPCTR ODR Accuracy

Could you please provide information about the output data rate (ODR) for the IIS2DLPCTR accelerometer?For example, if I want an ODR of 50Hz in High Performance mode, with BW=ODR/2, how accurate is the 50Hz ODR?  Similarly, if I use the single data c...

NBerr.1 by Associate II
  • 1728 Views
  • 3 replies
  • 0 kudos

calibration of accelerometer and gyro in lsm6d

we are using LSM6DSV16x sensor with nrf5340 dk board , wea are getting values like this ACC[mg]:x:-157.50,y:-30.74,z:981.00GYRO[mdps]:x:-700.00,y:-140.00,z:420.00,please help in calbration to get accurate values of  sensor .

AlgoBuilder for IKS01A2

Hi, I understand IKS01A2 is not supported anymore in the current AlgoBuilder software versionIs it still possible to download the last AlgoBuilder version that supports this board ?I can only download the latest version from the website (no older ver...

mtzt by Associate
  • 1101 Views
  • 1 replies
  • 0 kudos