Skip to main content
Palmering
Associate II
July 2, 2024
Solved

IIS3DWB: how to detect over range

  • July 2, 2024
  • 2 replies
  • 1873 views

Hi,

I'm using the IIS3DWB accelerometer to get triaxial waveform.

I just want to know what is the best approach to detect over range.
I tried to compare sample by sample in each channel with the maximum possible positive value (>32766) and the maximum negative value (<-32767) but I didn't get overflow detection when the peak acceleration > range.
When I set the limits to +/-16384 (half) my detection routine works (with an instantaneous acceleration value > range/2).

What is the measured acceleration value when the acceleration is over the full-scale range?
Does the accelerometer limit the the value to the maximum?

Best regards

 

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @Palmering ,

You can't detect over range, the maximum value you can read is the full-scale value.

2 replies

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
July 4, 2024

Hi @Palmering ,

You can't detect over range, the maximum value you can read is the full-scale value.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Palmering
PalmeringAuthor
Associate II
July 5, 2024

Hi Federica,

Thank you for your answer.

I think that comparing sample by sample, when at least a few of them reach the full-scale value (+ or -) of the range we can say there is an over range.

Based in your comment, I assume the IIS3DWB limits to the ful-scale value (0x7FFF/0x8000) if over range.
However, I couldn't see samples >=0x7FFB/<=0x8005. in the 16g range when a >16g shock.is applied.

Best regards