MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ASM330LHHX stops transmitting after some time.

I am using Nucleo F767ZI with SPI interface to ASM330LHHX sensor. I am using example code from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/asm330lhhx_STdC/examples/asm330lhhx_read_data_polling.cAfter a couple of second...

MAnto.2 by Associate III
  • 995 Views
  • 2 replies
  • 2 kudos

Resolved! L3gd20 sensor on stm32f411e-discovery

I am practicing reading L3GD20 data built into the stm32f411e-discovery kit. I use SPI1 to communicate with L3GD20. I watched on YouTube, they have instructions on how to use the void function HAL_GPIO_EXTI_Callback. I cannot call the void HAL_GPIO_E...

image.png image.png image.png image.png

LSM303AGR temperature measurement

Hi everybody,I'm using a LSM303AGR and I got some difficulties to read the temperature.My I2c functions, because I can read "who am I" registers, and I tried to write then to read some registers. I did the following steps :     LSM303_IO_Write_one_by...

LSM303.png
fab04 by Associate III
  • 800 Views
  • 1 replies
  • 0 kudos

LPS25HBTR_Recommended Land pattern

Hi Team,In our design we planned to use this part LPS25HBTR (Pressure sensor). As per Datasheet Recommended land pattern is not available. Could you please share PCB land pattern for this part LPS25HBTR. Thanks & Regards,Karthikeyan

LIS2MDL - impact to ODR When Set_FREQ = 1

Hi  Can someone clarify how long it takes for the sensor to temporarily stop reading, execute the SET pulse, and begin conversion when Set_FREQ is set to 1 in CFG_REG_B (61h) while in continuous conversion mode? I noticed that this setting randomly c...

Indi by Associate
  • 666 Views
  • 1 replies
  • 0 kudos

LIS2MDL OSR rate

HelloDoes anyone know the signal Oversampling Rate/s?I'm working for a Medtech company developing a novel device and we are thinking of using the LIS2MDL for our analysis. The data from the sensor will be analysed using different signal processing te...

Indi by Associate
  • 830 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSO(X) FSM Threshold Confusion

Hi all,This should be a question with a simple answer, but for some reason, I cannot find clarification. I am trying to use the Finite State Machine in the LSM6DSOX, and I have come across these examples below in this application note:I'm confused on...

Screenshot 2024-03-15 095604.png
jspear by Associate II
  • 794 Views
  • 1 replies
  • 1 kudos