MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FP-SNS-DATALOG2 and macOS

I recently updated to a macOS and am have downloaded FP-SNS-DATALOG2 function pack and was going to use the HSDPython_SDK to log data from my STEVAL-STWINBX1, however it appears that macOS is not supported, is that correct?  No love for macOS or am I...

WP by Associate III
  • 1463 Views
  • 2 replies
  • 0 kudos

imu data synchronization

Hello, I'm working with the lsm6do. The lsm6dso is configured to 6,67kHz sampling rate of both, acceleration and gyro data. The INT1 pin will be set if gyro and/or acc data is available (INT1_CTRL = 0x03). In my application I'm polling the int1 pin (...

K-laus by Associate
  • 718 Views
  • 0 replies
  • 0 kudos

LIS2DUXS12 Qvar and Interrupts

Hi all,I am trying to implement the  LIS2DUXS12 into a design and I am wondering if it is possible to still use the interrupts while using the Qvar sensors. Ideally, I need a way to detect when the device is on the human body and also a way to wake u...

Eyurk by Associate
  • 699 Views
  • 1 replies
  • 0 kudos

LIS2DW12 - Changing FIFO mode from bypass to cont-to-fifo

GreetingsI am running an application where I am using the LIS2DW12 accelerometer. I am using it for classical sampling of acceleration values in cont-to-fifo mode, which works fine. The FIFO is configured with the High pass filter enabled. I now want...

ZAIDS-S23 by Associate III
  • 1319 Views
  • 2 replies
  • 0 kudos

LIS3DH sensor data offset/value problems

We have designed the LIS3DH onto a custom PCBA, and we are seeing some oddities with the sensor readings post manufacturing. The PCBA goes into a two part injection molded enclosure made of ABS, and the two halves are ultrasonically welded together. ...

LSM6DSR use FIFO mode read data failed

I use LSM6DSR,  I set Accelerometer ODR selection can read data, but i choose fifo mode to read data, i don't read data, i set CTRL3_C is 0x01, CTRL1_XL is 0x50,  CTRL3_C is 0x40, CTRL5_C is 0x20, CTRL9_XL is 0xf8, INT1_CTRL is 0x01, INT2_CTRL is 0x0...

sunyu by Associate
  • 868 Views
  • 1 replies
  • 0 kudos

ISM330DLC Lifecycle

Hi all,I wanted to get information on the lifecycle of the ISM330DLC device? Is there a certain date when the sensor values will drift outside of the allowable tolerances? Thank you,Imran

IKalh.1 by Associate II
  • 1606 Views
  • 4 replies
  • 0 kudos

Using X-CUBE-MEMSMIC1 without X-NUCLEO-CCA02M1

Hello, I am trying to record audio with external digital PDM microphones using the MEMSMIC1 example but it is not so straightforward without the nucleo expansion board. Because the CCA02M1 has a direct connection to the pc it is able to be detected a...

BLE connection allmems 1 v4.2.0 - Sensortile

Hello, I'm using a STEVAL-STLKT01V1 demo board to perform voice streaming over BLE using allmems 1 v4.2.0 (since versione 4.3.0 dropped support for my demo board). My setup is:Steval demo board with allmems v4.2.0Python script using Bleak library to ...