MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HH single/multiple Read on I3C

since LPS22HH support one byte read or multiple byte read. wonder how LPS22HH handles the last bit on I3C because last bit in Read data is 'T', rather than ACK/NACK from I3C Controller. How does LPS22HH (target) know Controller need single or mulitpl...

wenge by Associate
  • 477 Views
  • 0 replies
  • 0 kudos

6 pdm microphones with MEMSMIC1 example

Hello, I am currently running the MEMSMIC1 audio streaming example via usb with 4 channels and it works fine, but Because i am using the nucleo-wb55 board that has a pdm interface supporting up to 3 microphone pairs I want to use as many microphones ...

Resolved! LIS344ALH Pspice model

Hello everyoneI need to have the pspice model of LIS344ALH (i know that this product is not longer available)I try do it with the datasheet but i don't have enought infoCan someone help with it ? :)Thanks ;)

fru999 by Associate III
  • 1383 Views
  • 4 replies
  • 0 kudos

ASM330LHH

hello,     i'm working on ASM330LHH IMU sensor, here raw value is continuously fluctuating even sensor is in untouch condition(fluctuation is between -1 to 6). is it possible to make it zero? so how can i stop this fluctuation. plz share suggetions o...

IIS2DLPC 6D orientation detection not working

Hi,I have attempted to follow the AN5201 application note page 26 to configure the IIS2DLPC accelerometer to generate an interrupt at every threshold however this interrupt is never generated. I have tried to print the value of SIXD_SRC register and ...

msingh08 by Associate III
  • 744 Views
  • 1 replies
  • 0 kudos

Resolved! IIS3DWB - ODR Accuracy

Hello,I am working with the IIS3DWB for a vibration monitoring sensor, and have a few questions about the ODR (Output Data Rate) accuracy, hoping someone can help me.1. I know that on the datasheet the ODR accuracy is stated as +-1% typ, or +-2% Max....

Wellett by Associate
  • 1156 Views
  • 2 replies
  • 1 kudos

Resolved! SensorTile.box Pro and External Power Supply

Hi,I want to run an application for a week. This video says the battery life is 10 hours:https://youtu.be/gFkIcrUkP5w?t=452s Question:Can I use an external power supply like this and set it to 5v:https://www.adafruit.com/product/4880 Connect it's bar...

Williamx by Associate
  • 781 Views
  • 1 replies
  • 0 kudos

Resolved! MTBF value for ASM330LHHTR

Hi,I am trying to calculate the MTBF (mean time between failures) value for the ASM330LHHTR module. Please suggest any techniques for the same. I am currently using the Qjc (Junction to Case Thermal Resistance) and Pd (Power Dissipation) values to ca...