User Activity

I use LIS2DS12 This is my init function   void LIS2DS12_Init(void) { uint8_t ctrl_1 = 0x72; //0111 for 6.4kHz ODR [7:4], 00 for 2g [3:2], 1 for high frequency available[1], 0 for BDU not activated [0] uint8_t ctrl_2; // [6] for soft_reset, [1] for ...
Hey everyone, I am working with the ADXL 354 eval board with an STM32H745data sheet ADXL354 : https://www.analog.com/media/en/technical-documentation/data-sheets/adxl354_adxl355.pdfdata sheet eval boad: https://www.analog.com/media/en/technical-docum...
Hi everyone I can find help on how to connect SPI2 STM32H745. I have read the datasheet and did everything written on it.Please can someone help me 
Hi everyonethis is my code for reading X axis ADXL355 accelerometer thanks to STM32h745.But when I run it, i keep being stuck if the HAL-SPIèTransmitReceive Can you help me ?
Hi everyone, I am trying to use an accelerometer with my STM32h745 board thought SPI.DO you have any idea where I can find library for thus accelerometers ?And how to use the SPI protocole with STM32H745 :)