2011-12-29 2:04 AM
Hi,
I intend to use several STeval-MKI109Vx structures, up to ten systems, simultaneously, andall of them ''wireless''. STM offers a wireless Bluetooth kit for connecting to STeval-MKI109V1.Is it possible to use up to 10 evalboards simult. with BT or would it be better to use ZigBee?For example modules based on STM32W108xx.Eventually these modules could be used without other uC, only by using the host W108xxand adding a inertial sensor.These should be ''streaming'' wireless nodes. thank's for answers