MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303DLM

Posted on September 08, 2011 at 11:23Hi all, I'm working with LSM303DLM. I have read successfully accelerometer and magnetometer value. Now, i want to use LSM303DLM module as a wakeup device. When my motorbike don't move, the MCU goes to Standby mod...

LIS331HH z-Acc is always zero

Posted on March 19, 2012 at 14:39Hi, i wanna access the acceleration values for the x,y,z axis. So i get a response and values from the registers x (0h28,0h29) and y (0h2A,0h2b), but the register for the z accelerations (0h2C,0h2D) is always zero. A...

iNemo firmware package v2.2.0 hex file

Posted on May 31, 2012 at 18:17Hi, I have been using for some time original iNemo suite application and DFU mode, then I made another program and uploaded it with JTAG programmer.How can I use iNemo suite again?, uploading iNEMOV2_Firmware_PackageV2...

miego by Associate
  • 693 Views
  • 2 replies
  • 0 kudos

legal rights about SDK code

Posted on May 22, 2012 at 23:54Hi, is it allowed to upload the firmware of my custom inemo application (sportmeter), which based on the SDK of STmicro   to sourceforge ? WR Alex

L3G4200D angle calculation

Posted on May 24, 2012 at 14:47Hi there,I'm using an L3G4200D sensor for calculating the angle displacementwith the code below. However from the computation I get half of the real rotationthe sensor make, that is, if I rotate it of 90 degree, I meas...

iNEMO 2.x Project in Keil µVision

Posted on April 24, 2012 at 15:38Hi, ist their any iNemo Project already ported in KEIL ? I'm searching for a solution to use the IAR Project in Keil but I always failing when i trying it by my self. with regards Sam

working with multiple INEMO cards in a MATLAB script

Posted on May 04, 2012 at 14:05hello all! I  am working on my final project in ee studies, and my project requires getting input measurements from 2 INEMO V1 cards at the same script in a MATLAB enviorment. can it be done? and if so, how can I do it...

yakir by Associate
  • 570 Views
  • 0 replies
  • 0 kudos

ST denied access to download iNEMO Lite Engine

Posted on April 09, 2012 at 10:25I bought both of the iNEMO Eval boards v1 & v2. I have been working with them. Recently i found ST is released 'iNEMO Lite Engine', i registered for downloading. ST reply is below:Dear valuable customer,After interna...

harinath by Associate III
  • 662 Views
  • 2 replies
  • 0 kudos

How do I acquire the iNemo Drivers for Windows 8

Posted on April 18, 2012 at 19:44In the past three weeks I've filled out the form for requesting the iNemo drivers for Windows 8 twice, and have contacted support and they've put me in contact with two different non-responsive sales people (that hav...

joel2399 by Associate
  • 597 Views
  • 0 replies
  • 0 kudos

Why AHRS Update rate is 50Hz when STM32 can work at 72MHz ?

Posted on April 06, 2012 at 09:35I don't understand why AHRS updated only at 50Hz when STM32F103xx can work at 72MHz.I want to reprogram iNEMO v2 board to change the AHRS update rate to 200Hz. What limits STM32 to update AHRS at only 50Hz.I'm workin...

harinath by Associate III
  • 1157 Views
  • 4 replies
  • 0 kudos