MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH noise characteristics

Posted on September 14, 2012 at 16:03Dear all, I am using the LIS3DH configured with 1.25 kHz bandwith (ODR) and high resolution (12bits), full scale range of +/- 2g. I have a question regarding the noise I should expect at this frequency : The data...

SETVAL interface to STM32 DISCOVERY

Posted on September 15, 2012 at 15:18I apologize right now for my English. I purchased a STM32VLDISCOVERY and unsteval-mki0 +2 v2 both st microelectronics. I tried the program that is given with the second component, and seemed very nice. Wanted ho...

nico23 by Senior III
  • 542 Views
  • 0 replies
  • 0 kudos

Problem with iNEMO2_SDK_Wrapper.cs

Posted on August 28, 2012 at 12:01I'm trying to use the V2 board as a sensor board for own experiments with sensor fusion using C# (in VS Express 2010) But I already have the problem, that the debugger throws me out of the Wrapper in the Connect-fun...

L3DG20/LSM303DLHC ''block data update''

Posted on August 10, 2012 at 22:01I was reading through the documentation on these and saw the ''block data update'' feature, obviously useful because it's two 8-bit registers and it might be possible for the data to update between reads and thus no...

dannym by Associate III
  • 779 Views
  • 0 replies
  • 1 kudos

LPR430AL roll angle wrong

Posted on August 07, 2012 at 14:38I work with the gyroscope LPR430AL. The pitch angle works fine, the roll angle results in some strange values... (if I turn the module of 90° in roll angle I measure the right value of 90°. When I come back to 0°...

iNemo Lite code's interface?

Posted on July 06, 2012 at 19:45I have the iNEMO Lite code for its Extended Kalman filter.  I have a board I made with an LSM303DLM and LSM330DL connected to the STM32F4 Discovery board for the IMU.Is there any example?  It looks like it's a library...

dannym by Associate III
  • 661 Views
  • 1 replies
  • 0 kudos

Inprove the speed of the ''Mass storage'' as u disk

Posted on March 13, 2012 at 09:30hello everybody,  I was tested using the TF card as a U disk routines.The read speed is 500KB-700KB / s, write speed of 100KB/ s. Too slow, I would like to increase its transmission speed.I will change the way of the...

power3347 by Associate II
  • 3289 Views
  • 15 replies
  • 0 kudos

lsm330dl accelerometer output data problem

Posted on July 03, 2012 at 06:04i'm using the accelerometer in lsm330dl. but when i put the chip statically on the table, the xyz output i got from it is very strange,  for x, it's always between 0.2-0.45  for y, it's always around 1  for z, it's al...