MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303D anti-alias filter

Posted on October 31, 2014 at 21:54I'm a bit lost about the use of the acceleration filter bandwidth. How to choose the relevant value between 50 and 773Hz ? -- Fabien #filter #lsm303d #accelerometer

how get INEMO software demonstration?

Posted on October 22, 2014 at 11:41how get INEMO software demonstration, the server seem out of order, I try 6 times I receive, illegal character and after the server is out of order, try later

yves2399 by Associate II
  • 730 Views
  • 0 replies
  • 0 kudos

iNEMO Engine M1 LI3 - ported to STM32F4 not showing coorect data

Posted on October 22, 2014 at 08:18Hello, i am using the iNEMO Lite soft version, namely INEMOEngineM1LI3,  the only thing i modified to work with the stm32f407 was some i2c functions, and the data/trafic on the i2c buss is ok. I tryied to display t...

Bogdan by Senior
  • 840 Views
  • 0 replies
  • 0 kudos

LIS3DSH SPI + resolution

Posted on October 21, 2014 at 10:33Hi, I have one question about the SPI of the LIS3DSH sensor. Does it have a multiple byte read bit? On page 26/53 (datasheet) in figure7 there is a MS bit, but in the text it is not mentioned. Where is the mistak...

truland by Associate
  • 881 Views
  • 0 replies
  • 0 kudos

PC Unable to Recognize STEVAL-MKI138V3

Posted on October 20, 2014 at 21:02My computer is unable to see this USB device listed in the device manager. The documentation seems to suggest that its something that will be automatically recognized however that is not happening. I have tried eve...

Usage of STEVAL-MKI126V1 & STEVAL-MKI138V1

Posted on October 17, 2014 at 10:26Dear all,I working on a audio project where  a microphone memes array is used to record environmental audio. I want to use STEVAL-MKI126V1 and STEVAL-MKI138V1. On the datasheet for STEVAL-MKI138V1 I saw that such a...

LSM9DS0 examples using STSW-MEMS031?

Posted on October 10, 2014 at 20:19Hi All,I'm trying to find either documentation, or example code on using the device drivers in STSW-MEMS031. Does something like this exist?  The ZIP file only contains the two C files and a header.Thanks!

H3LIS331DL

Posted on October 14, 2014 at 15:32Hi,  I wonder if anyone can help with a sleep / interrupt problem?  When the sensor is awake and with the registers set for our application the device generates interrupts as expected.  If we change just the sleep ...