cancel
Showing results for 
Search instead for 
Did you mean: 

will it measure liquid level in mm accuracy?

kudiarasum
Associate II
Posted on October 27, 2014 at 09:43

Hi,

we can get mm accuracy in diesel level measurement?  

#vl6180x #proximity-sensor
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Colin RAMRATTAN
Associate II
Posted on October 27, 2014 at 17:03

Hello,

To answer  your question, yes we can detect diesel within the same performance as outlined in the VL6180X datasheet. As diesel is not 100% clear the VL6180X will report a distance. If the liquid is clear or slightly clear then we cannot guarantee the measurement readback from the VL6180X.

Thanks,

Colin

Julien NGUYEN
ST Employee
Posted on October 27, 2014 at 17:23

Hello,

We noticed that it depends on the reflectivity of the tank bottom.

We could measure with precision the black body tank bottom but it didn't work with the white bottom.

Regards,

Julien


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.